IL.KPDRATIO

General Information

Type

NV Parameter

Description

Sets the proportional gain of the d-component current PI-regulator as a percentage of IL"Instruction list" This is a low-level language and resembles assembly.KP

Units

N/A

Range

0 to 100

Default Value

1

Data Type

Float

See Also

IL.KP

Start Version

M_01-00-00-000

Description

This parameter modifies the proportional gain of the PI-loop, which controls the d-component of the current.

Related Topics

1    Current Loop

 


Stay Connected with Kollmorgen

Copyright © 2015 Kollmorgen™