MOTOR.KE

General Information

Type

NV Parameter

Description

Sets the motor back EMF constant.

Units

Vpeak/krpm for Rotary Motors

Vpeak/m/s for Linear Motors

Range

0.0 to 100,000

Default Value

0

Data Type

Float

See Also

N/A

Start Version

M_01-03-06-000

Description

MOTOR.KE defines the back EMF constant for the motor. The back EMF constant defines how much voltage is generated at the motors coils. The relationship between MOTOR.KE and speed is described by the following equation:

Coil Voltage = MOTOR.KE * VL.FB

VL.FB is in units of krpm for rotary motors and in units of m/s for linear motors.

The maximum speed for interior permanent magnet motors (IPM) is determined by MOTOR.KE and VBUS.VALUE. An overspeed fault is generated if MOTOR.TYPE is set to 6 (IPM) and VL.FB * MOTOR.KE exceeds VBUS.VALUE.

Related Topics

Motor | VL.FB | VBUS.VALUE

 


Stay Connected with Kollmorgen

Copyright © 2015 Kollmorgen™