Open topic with navigation
General Information
Type
R/O Parameter
Description
Reads the motor temperature represented as the resistance of the motor PTC or NTC.
Units
Ω
Range
0 to 232 Ω
Default Value
N/A
Data Type
Integer
See Also
Start Version
M_01-00-00-000
This parameter returns the motor temperature, which is represented as the resistance of the motor's PTC or NTC.
Related Topics
Motor | MOTOR.RTYPE
Stay Connected with Kollmorgen
Copyright © 2015 Kollmorgen™