|
General Information |
|
|---|---|
|
Type |
NV Parameter |
|
Description |
|
|
Units |
Ω |
|
Range |
0 to 2,000,000,000 Ω |
|
Default Value |
0 Ω = switched off |
|
Data Type |
Integer |
|
See Also |
|
|
Start Version |
M_01-00-00-000 |
Description
This parameter is used to configure the motor temperature fault level as a resistance threshold of the motor thermal sensorA sensor is a type of transducer that converts one type of energy into another for various purposes including measurement or information transfer.
A zero value prevents any fault from being issued.
For firmware versions 01-09-00-000 and later, this parameter is automatically configured for Kollmorgen motors when MOTOR.AUTOSET = 1.
Related Topics
|
Copyright © 2015 Kollmorgen™ |
|