DRV.HWENDELAY

General Information

Type

NV Parameter

Description

Delay time between inactive Hardware EnableEnable signal for the drive, Hardware-Enable with 24V signal to X8, Software-Enable command by setup Software, fieldbus or permanently set. Both are required for enabling the drive. input and drive disable.

Units

Milliseconds

Range

0 to 167 ms

Default Value

0 ms

Data Type

Integer

Start Version

01-05-08-000

FieldbusA Fieldbus is an industrial network system for real-time distributed control (e.g. CAN or Profibus). It is a way of connecting instruments in a plant design

Index/Subindex

Object Start Version

EtherCATEtherCAT is an open, high-performance Ethernet-based fieldbus system. The development goal of EtherCAT was to apply Ethernet to automation applications which require short data update times (also called cycle times) with low communication jitter (for synchronization purposes) and low hardware costs COE and CANopen

5264h/0

M_01-05-08-000

Description

By default, when the Hardware DisableRemoval of the ENABLE signal. Disables power stage. input deactivates, the drive is immediately disabled. However, on a vertical axis this may allow the load to drop slightly before the brake is applied.

To ensure that the brake is applied before the power stage is disabled, set DRV.HWENDELAY to a value which allows the brake to apply fully.

While the brake is applying, the drive will also attempt to decelerate the motor using the standard drive disable settings such as DRV.DISMODE, CS.DEC, CS.VTHRESH and CS.TO.

Related Topics

DRV.DISMODE | CS.DEC | CS.VTHRESH | CS.TO | MOTOR.TBRAKEAPP

 


Stay Connected with Kollmorgen

Copyright © 2015 Kollmorgen™