|
General Information |
|
|---|---|
|
Type |
NV Parameter |
|
Description |
Sets the proportional gain of the d-component current PI-regulator as a percentage of IL"Instruction list" This is a low-level language and resembles assembly.KP |
|
Units |
N/A |
|
Range |
0 to 100 |
|
Default Value |
1 |
|
Data Type |
Float |
|
See Also |
|
|
Start Version |
M_01-00-00-000 |
|
Index/Subindex |
Object Start Version |
|
|---|---|---|
|
3596h/0 |
M_01-00-00-000 |
Description
This parameter modifies the proportional gain of the PI-loop, which controls the d-component of the current.
Related Topics
|
Copyright © 2015 Kollmorgen™ |
|