IL.KPLOOKUPVALUES

General Information

Type

R/W Parameter

Description

Gets the Current Loop Gain Scheduling Table.

Units

N/A

Range

N/A

Default Value

N/A

Data Type

Table

See Also

IL.KPLOOKUPINDEX, IL.KPLOOKUPVALUE, IL.KP

Start Version

M_01-04-00-000

Description

Retrieves the Current Loop Gain Scheduling Table in a comma delimited table.

This table is 256 records long, and the table will return values in the following format:

-->IL.KPLOOKUPVALUES

Index Value

0, 100.000

1, 100.000

2, 100.000

3, 100.000

4, 100.000

5, 100.000

6, 100.000

7, 100.000

8, 100.000

9, 100.000

10, 100.000

Related Topics

Current Loop

 


Stay Connected with Kollmorgen

Copyright © 2015 Kollmorgen™