MOTOR.BRAKEIMM

General Information

Type

NV Parameter

Description

Brake Immediately: in the case of a drive disable, apply the brake as soon as the power stage disables.

Units

N/A

Range

0 to 1

Default Value

0 (Inactive)

Data Type

Boolean

See Also

N/A

Start Version

M_01-05-11-000

FieldbusA Fieldbus is an industrial network system for real-time distributed control (e.g. CAN or Profibus). It is a way of connecting instruments in a plant design

Index/Subindex

Object Start Version

EtherCATEtherCAT is an open, high-performance Ethernet-based fieldbus system. The development goal of EtherCAT was to apply Ethernet to automation applications which require short data update times (also called cycle times) with low communication jitter (for synchronization purposes) and low hardware costs COE and CANopen

5268h/0

M_01-05-11-000

Description

Sets the brake to apply as soon as the power stage disables. The brake will not apply immediately when the disable command is issued, but at the point when the power stage actually disables. The power stage can disable due to user command (DRV.DIS), digital input, fieldbus, STO, or fault. The point at which the power stage disables depends on the disable mode settings or type of fault for each case.

Value Description
0 Inactive
1 Brake as soon as power stage disables.

Related Topics

Motor | DRV.DISMODE | CS.VTHRESH  | CS.TO | MOTOR.TBRAKETO | DRV.DISTO

 


Stay Connected with Kollmorgen

Copyright © 2015 Kollmorgen™