|
General Information |
|
|---|---|
|
Type |
R/W Parameter |
|
Description |
|
|
Units |
ms |
|
Range |
100 to 20,000 |
|
Default Value |
1000 |
|
Data Type |
U16 |
|
Start Version |
M_01-06-07-000 |
|
Index/Subindex |
Object Start Version |
|
|---|---|---|
|
535Ch/0 |
M_01-06-07-000 |
Description
In Wake & Shake mode 1, a maximum current of WS.IMAX is applied to the motor. WS.TSTANDSTILL defines a wait time, during which this maximum current is held, before detecting the commutation angle of the motor. Longer times are useful for big inertia motors or heavy loads.
Related Topics
Wake and Shake Overview | WS.MODE | WS.TIRAMP
|
Copyright © 2015 Kollmorgen™ |
|