FunctionMLAxisGenReadDecPipe Network motion icon

Description

Get the Deceleration of the internal generator of an axis.

Arguments

Input

AxisID

Description

ID Name of the Axis block

 

Data type

DINT

 

Range

 

Unit

n/a

 

Default

Output

OK

Description

 

 

Data type

BOOL

 

Unit

n/a

Deceleration

Description

Returns Axis Deceleration value

 

Data type

LREAL

 

Unit

User unit/sec2

Related Functions

MLAxisGenReadAcc

MLAxisGenReadSpd

Example

Structured Text

 

Axis1_Deceleration := MLAxisGenReadDec( PipeNetwork.Axis1 );

 

Ladder Diagram

MLAxisGenReadDec: LD example

Function Block Diagram

MLAxisGenReadDec: FBD example

(missing or bad snippet)

 


Stay Connected with Kollmorgen

Copyright © 2018 Kollmorgen