MLCNVConECAT
Description
This function will connect the output of a pipe convertor block to an EtherCATEtherCAT is an open, high-performance Ethernet-based fieldbus system. The development goal of EtherCAT was to apply Ethernet to automation applications which require short data update times (also called cycle times) with low communication jitter (for synchronization purposes) and low hardware costs Output (Rx) PDO object. The output value of the convertor block will then be written to the PDO object every update of the convertor block. The pipe block is specified by the BlockID input and the PDO object is specified by the DeviceAddr, Index, and SubIndex inputs.
Arguments
Input
| BlockID | Description | The convertor block whose output value will be written to the PDO object. For example: PipeNetwork:CNV1 |
| Data type | DINT | |
| Range | n/a | |
| Unit | n/a | |
| Default | — | |
| DeviceAddr | Description | The device address of the PDO object to be written. EtherCAT devices are numbered in order with the first device being 1001, the second 1002, etc. |
| Data type | INT | |
| Range | n/a | |
| Unit | n/a | |
| Default | — | |
| Index | Description | The index of the PDO object to be written. The index can be determined from the table located in the “PDO Selection/Mapping” tab of the EtherCAT device page. (In Project Explorer, under EtherCAT, select the device, then select the PDO Selection/Mapping tab.) |
| Data type | UINT | |
| Range | n/a | |
| Unit | n/a | |
| Default | — | |
| SubIndex | Description | The sub index of the PDO object to be written. The sub index can be determined from the table located in the “PDO Selection/Mapping” tab of the EtherCAT device page. (In Project Explorer, under EtherCAT, select the device, then select the PDO Selection/Mapping tab.) |
| Data type | USINT | |
| Range | n/a | |
| Unit | n/a | |
| Default | — |
Output
|
Default (.Q) |
Description | Returns TRUE if this function has successfully connected
the output of the pipe convertor block to the
EtherCAT Output (Rx) PDO Object.
See more details here |
| Data type | BOOL | |
| Unit | n/a |
Related Functions
Example
Structured Text
//Connect a converter Pipe Block named “CNV2” to PDO 16#60B2 (Accel FF) on ECAT address 1002.
MLCNVConECAT( PipeNetwork.CNV2, 1002, 16#60B2, 0 );
Ladder Diagram
Function Block Diagram
|
Copyright © 2018 Kollmorgen |
|