GetCtrlPerf

Description
This function block returns controller CPU performance statistics.
See also:
Arguments
Input
| Execute | Description | On the rising edgeA rising edge is the transition of a digital signal from low to high. It is also called positive edge, request to collect the controller's performance data. |
| Data type | BOOL | |
| Range | 0,1 | |
| Unit | n/a | |
| Default | — | |
| DataPointCount | Description | The number of motion manager cycles over which performance statistics will be gathered. |
| Data type | UDINT | |
| Range | 2 - 240,000 | |
| Unit | n/a | |
| Default | — |
Output
| Done | Description | If True, then the command completed successfully. |
| Data type | BOOL | |
| Error | Description | If True, an error has occurred. |
| Data type | BOOL | |
| ErrorID | Description | Indicates the error if Error output is set to TRUE.ErrorID = 0 indicates no error, ErrorID = 1 indicates an error |
| Data type | INT | |
| MissedCycles | Description | Indicates the number of missing VM cycles. |
| Data type | UDINT | |
| MeanVmTime | Description | The mean VM execution time measured in microseconds. |
| Data type | LREAL | |
| StdDevVmTime | Description | The standard deviation of the VM execution time measured in microseconds. |
| Data type | LREAL | |
| MinVmTime | Description | The minimum VM execution time measured in microseconds. |
| Data type | LREAL | |
| MaxVmTime | Description | The maximum VM execution time measured in microseconds. |
| Data type | LREAL | |
| MeanMotMgrTime | Description | The mean motion manager execution time measured in microseconds. |
| Data type | LREAL | |
| StdDevMotMgrTime | Description | The standard deviation of the motion manager execution time measured in microseconds. |
| Data type | LREAL | |
| MinMotMgrTime | Description | The minimum motion manager execution time measured in microseconds. |
| Data type | LREAL | |
| MaxMotMgrTime | Description | The maximum motion manager execution time measured in microseconds. |
| Data type | LREAL | |
| MeanCpuIdlePct | Description | The mean percentage of time the controller CPU is idle. CPU idle period is measured across all CPU cores.
|
| Data type | LREAL | |
| StdDevCpuIdlePct | Description | The standard deviation of the measurements of the time that the controller CPU is idle. CPU idle period is measured across all cpu cores.
|
| Data type | LREAL | |
| MinCpuIdlePct | Description | The minimum measurement of the time that the controller CPU is idle. CPU idle period is measured across all cpu cores.
|
| Data type | LREAL | |
| MaxCpuIdlePct | Description | The maximum measurement of the time that the controller CPU is idle. CPU idle period is measured across all cpu cores.
|
| Data type | LREAL |
Example
FBD
FFLD
Structured Text
//Read controller performance data from last 1000 cycles (1 second at T#1ms update rate)(missing or bad snippet)
Inst_GetCtrlPerf( ReadPerformanceData, 1000 );
IF Inst_GetCtrlInfo.Done THEN
MissedCycles:= Inst_GetCtrlPerf.MissedCycles;
MaxVmTimeMs:= Inst_GetCtrlPerf.MaxVmTime;
MaxMotionManagerTime:= Inst_GetCtrlPerf.MaxMotMgrTime;
MeanCPUIdlePercentage:= Inst_GetCtrlPerf.MeanCpuIdlePct;
MaxCPUIdlePercentage:= Inst_GetCtrlPerf.MaxCpuIdlePct;
END_IF;
|
Copyright © 2018 Kollmorgen |
|