FunctionMLGearWriteOffPipe Network motion icon

Description

Sets the Offset value of a selected Gear Pipe Block.

The output of a Gear Block = Input value * Ratio + Offset


  • Values lower then 1.0 can be entered, but require a leading zero (for example 0.8 instead of .8)

Arguments

Input

BlockID

Description

ID number of an initialized Gear Pipe Block

 

Data type

DINT

 

Range

[-2147483648, 2147483648]

 

Unit

n/a

 

Default

Offset

Description

New Offset value to be assigned to selected Gear Pipe Block. Values lower then 1.0 can be entered, but require a leading zero (for example 0.8 instead of .8)

 

Data type

LREAL

 

Range

 

Unit

User unit

 

Default

Output

Default (.Q)

Description

Returns TRUE if Offset value is changed in the selected Gear Pipe Block

See more details here

 

Data type

BOOL

 

Unit

n/a

Return Type

BOOL

Related Functions

MLGearReadOffset

MLGearInit

Example

Structured Text

 

//Set the Offset value of Gear1 Pipe Block to 5 User Units

MLGearWriteOff(PipeNetwork.GEAR1, 5.0);

 

Ladder Diagram

MLGearWriteOff: LD example

 

Function Block Diagram

MLGearWriteOff: FBD example

(missing or bad snippet)

 


Stay Connected with Kollmorgen

Copyright © 2018 Kollmorgen