MLPmpRun
Description
Jog the generator at the requested speed.
Arguments
Input
| EN | Description |
Enables FB to be executed. |
| Data type |
BOOL |
|
| Range |
0, 1 |
|
| Unit |
n/a |
|
| Default |
— |
|
| BlockID | Description |
ID Name of the PMP function block in the Pipe Network |
| Data type |
DINT |
|
| Range |
[-2147483648, 2147483648] |
|
| Unit |
n/a |
|
| Default |
— |
|
| Speed | Description |
The desired rate at which to Jog. If the speed is 0.0 User Units / second the PMP block decelerates to zero speed and switches to the Idle state (0). |
| Data type |
LREAL |
|
| Range |
— |
|
| Unit |
User unit/sec |
|
| Default |
— |
Output
|
Default (.Q) |
Description |
Returns True if the MLPmpRun successfully completed. See more details here |
| Data type |
BOOL |
|
| Unit |
n/a |
Related Functions
Example
Structured Text
//Execute a Relative move on a PMP Block name “PmpMaster” with a Jog speed of 1000.0
MLPmpRun( PipeNetwork.PmpMaster, 1000.0 ) ;
Ladder Diagram
Function Block Diagram
|
Copyright © 2018 Kollmorgen |
|