MLPhaReadSlope
Description
Get the phase slope value of a phaser block.
Arguments
Input
|
BlockID |
Description |
ID Name of a Phaser function block in the Pipe Network |
|
Data type |
DINT |
|
|
Range |
[-2147483648, 2147483648] |
|
|
Unit |
n/a |
|
|
Default |
— |
Output
|
Slope |
Description |
Present Slope value |
|
Data type |
LREAL |
|
|
Unit |
User unit/sec |
|
|
Default |
Value defined in the setup of a Phaser Block within a Pipe Network. Depending on the phase slope type setting, it is the VALUE in “PHASE_SLOPE_USER”, “PHASE” or the max slope. |
Related Functions
Example
Structured Text
|
PresentSlope :=MLPhaReadSlope( PipeNetwork.PhaseAdjust );
|
Ladder Diagram
Function Block Diagram
|
Copyright © 2018 Kollmorgen |
|