MLProfileCreate

Description
Creates a new Profile Object for use in a PLC"Programmable Logic Controller" A Programmable Logic Controller, PLC, or Programmable Controller is a digital computer used for automation of industrial processes, such as control of machinery on factory assembly lines. Used to synchronize the flow of inputs from (physical) sensors and events with the flow of outputs to actuators and events Program or Pipe Network CAM block. This function block is automatically called if a Profile is created in the Project Explorer, with user-defined settings then entered in the CAM Profile Properties screen.
Profiles are created and initiated separately and the shape is modified with the CAM Editor. With the Editor profiles can be changed graphically or by manually changing values in a numeric table relating input and output values with specific slopes. The Cam Editor software tool provides the capability to visualize, analyze, edit, and smooth profiles.
Profile switching can be done on the fly, without losing synchronization and without dead time. In addition, the offsets and ratios of CAM Profiles can be changed on the fly.
-
-
Profile objects are normally created in the Project Explorer. Then you do not have to add MLCamInit function blocks to their programs. By right clicking the Profiles folder under the PLC->Motion Tree, you can select Add new profile. Parameters are entered directly in a pop-up window, and the code is then automatically added to the current project.
-
-
This function should be called after MLMotionInit is called and before MLMotionStart is called.
Arguments
Input
| Name | Description |
Name of initialized CAM Profile |
| Data type |
STRING |
|
| Range |
— |
|
| Unit |
n/a |
|
| Default |
— |
Output
| OK | Description |
Indicates the profile has been created See more details here |
| Data type |
BOOL |
|
| ID | Description |
Returns the ID number of the created CAM Profile |
| Data type |
DINT |
|
| Unit |
n/a |
Related Functions
Example
Structured Text
|
//Create a new Profile Profile_A := MLProfileCreate( 'Profile_A' );
|
Ladder Diagram
Function Block Diagram
|
Copyright © 2018 Kollmorgen |
|