Logical View
An automation system usually needs an organized hierarchy of controller systems to function and usually including the following items:
Summary
Click on an item to display its summary.
| Color Legend | Description |
|---|---|
| Blue Cell | Belongs to KAS |
| Green Cell | Kollmorgen products |
| White Cell | Third parties |
| Blue Text | Click on the item to display more info next to the table. |
I/O Engine
Operating System
Feedback
Gear Boxes
Mechanical Elements
A Human-Machine Interface is usually employed to communicate with PLCs for further automated control or emergency response
PLCs usually have built-in communications ports. These communication links are often used for Human-Machine Interface devices such as AKI panels.


A Programmable Logic Controller is a digital computer used for automation of industrial processes, such as control of machinery on factory assembly lines. It is used to synchronize the flow of inputs from (physical) sensors and events with the flow of outputs to actuators and events


For synchronizing axes that are linked to an external source (motor), the provides the capability to define the motion in 2 different ways: Pipe Network or PLCopen
.
.
- Pipe Network is a graphical method using channels between source objects and destination objects. The main application of the pipe concept is to describe motion profiles and other positional relationships.

- PLCopenA vendor -and product- independent worldwide association active in Industrial Control and aiming at standardizing PLC file formats based on XML is a standardized programming method to describe motion profiles.
The Fieldbus
is the industrial network system that controls the motion. Communicating frames requires high performance and reliability to ensure real-time distribution

is the industrial network system that controls the motion. Communicating frames requires high performance and reliability to ensure real-time distribution
Inputs are the signals or data received by the automation system, and Outputs are the signals or data sent from it.


A Drive is an electronic device to provide power to a motor or servo


Motors are mostly used when circular motion is needed, but can also be used for linear applications by transforming circular to linear motion with a bolt and screw transducer. Some actuators, however, are intrinsically linear

|
Copyright © 2018 Kollmorgen |
|