AKD PDMM and PCMM Hardware

The AKD PDMM comprises of three printed circuit boards (PCB"Printed Circuit Board" A PCB is used to mechanically support and electrically connect electronic components using conductive pathways, tracks or signal traces etched from copper sheets laminated onto a non-conductive substrate) while the PCMM comprises of one.

Figure 2-11: AKD PDMM and PCMM card


  • Please note that any reference to AKD PDMM or PCMM refers to both the 800MHz and the single- and dual-core 1.2GHz variants, unless otherwise noted.

 


Stay Connected with Kollmorgen

Copyright © 2018 Kollmorgen