ESI File Management

ESI files which are referenced from a project's EtherCATEtherCAT is an open, high-performance Ethernet-based fieldbus system. The development goal of EtherCAT was to apply Ethernet to automation applications which require short data update times (also called cycle times) with low communication jitter (for synchronization purposes) and low hardware costs devices are stored in the project.


  • The ESI files are stored along with the project so the project can easily be moved to another location and it will still compile. It still compiles because the ESI files are copied back to the local folder.


  • There is the possibility that the names and/or contents of files can be conflicting. The system checks the files before adding them. You will be prompted to chose the correct file should any conflicts be found.


  • WARNING: Replacing an ESI file changes the configuration of any associated device to the new file. You will be prompted to confirm or cancel replacing an ESI file and the associated devices' configurations.

ESI files will be replaced when: 

  • Opening a project file that contains an ESI file that is different from the file in the KAS Internal Library of ESI Files stored on the PC.
    • You are prompted to select "term_A" (use the version in the project) or "term_B" (use the ESI Internal Library version). Selecting "term_A" will overwrite the ESI Internal Library version.
  • Pressing the Add button in the ESI Files tab view and:
    • importing an ESI file name that already exists in the KAS Internal Library of ESI Files stored on the PC.
    • importing an ESI file that contains duplicate device information that already exists in the KAS Internal Library of ESI Files stored on the PC.

 


Stay Connected with Kollmorgen

Copyright © 2018 Kollmorgen