PDMM or PCMM B3 Button Menu

The B3 “Menu” push-button will cycle through a list of menu items displayed on the 7-segment LED. Pressing and holding the B3 button during the boot sequence (before the Boot Startup Script runs) provides access to a menu of functions. Each B3 press will advance to the next menu item. The menu item will be displayed for 10 seconds. Press B2 to select the current menu item. If no button is pressed within the 10 seconds, the 7-segment display will return to Normal operation.

Functionality Display Notes
Display the IP See Display the IP Address of a PDMM or PCMM
Start the application This will start the KAS RuntimeIn computer science, runtime (or run-time) describes the operation of a computer program, the duration of its execution, from beginning to termination (compare compile time). Within KAS, runtime also refers to the virtual machine that manage the program written in a computer language while it is running.
Factory Reset See Reset the Controller to Factory Settings
Backup firmware to SD card See Backup Using the B3 Button.
Restore firmware from SD card See Restore Using the B3 Button.

Table 7-3: Application is not running

Functionality Display Notes
Display the IP See Display the IP Address of a PDMM or PCMM
Stop the application This will stop the KAS Runtime.

Table 7-4: Application is running


  • Please note that when selected, the Start, Stop, Backup, Restore, and Reset functions do not initiate immediately; they require confirmation. The 7-segment displays flashes a "y", prompting for confirmation. Pressing B2 confirms the function and the process begins. If the function is not confirmed within 10 seconds the action is canceled.

 


Stay Connected with Kollmorgen

Copyright © 2018 Kollmorgen