Backup Tab
| Backup Controller |
This function is used to replicate a PCMM or the controller portion of the AKD PDMM. Clicking the button will save the data to the SD card. The 1.2 GHz single core RuntimeIn computer science, runtime (or run-time) describes the operation of a computer program, the duration of its execution, from beginning to termination (compare compile time). Within KAS, runtime also refers to the virtual machine that manage the program written in a computer language while it is running firmware file is optional. If provided, an 800 MHz single core model can be replaced with a 1.2 GHz single core model. If the 1.2 GHz single core Runtime firmware file is not included, then an 800 MHz single core model can only be replaced with another 800 MHz single core model.
After starting the Backup, an alert will be presented to confirm the backup should proceed. |
| Backup EtherCATEtherCAT is an open, high-performance Ethernet-based fieldbus system. The development goal of EtherCAT was to apply Ethernet to automation applications which require short data update times (also called cycle times) with low communication jitter (for synchronization purposes) and low hardware costs Devices |
This function replicates the network topology as well as the AKD, AKD PDMM, AKD-C, and AKD-N drives' unique ID, firmware and data. To accomplish the backup, a copy of the firmware package is required. There are several possible scenarios upon clicking this button.
For all other EtherCAT devices, such as couplers, IOs, ServoStar drives, and third-party devices, only the unique ID is backed up. |
-
-
Files on the website are saved in ZIP format. You must unzip the download to access the TGZ file.
|
Copyright © 2018 Kollmorgen |
|