Modifying the Type of a Cam Element

The type of element can either be a point or a line. The element type can be modified by double-clicking in the Type column of an element and then clicking on the down arrow. A list of choices is displayed as shown. Select the type of element from the list.

Modifying an Element Type

Figure 9-7: Modifying an Element Type

 


Stay Connected with Kollmorgen

Copyright © 2018 Kollmorgen