PDMM/PCMM EDS file for EtherNet/IP
The KAS installation contains an EtherNet/IP EDS file for the Kollmorgen controller. This file may be needed by other controllers, (PLCs, PCs etc.) to configure the EtherNet/IP communication with a AKD PDMM.
The KAS_Controller_EIP.eds file is located in the \Astrolabe\Bin\EDS directory, where the KAS software was installed. By default, the EDS file is located:
C:\Program Files (x86)\Kollmorgen\Kollmorgen Automation Suite\Astrolabe\Bin\EDS\KAS_Controller_EIP.eds
| Revision | Compatibility | Change |
|---|---|---|
| 1.0 | KAS v2.7 only | Initial revision |
| 1.1 | KAS v2.8 only | Updated vendor information |
| 1.2 | KAS v2.9 only | Support up to 4 input and output assemblies when KAS RuntimeIn computer science, runtime (or run-time) describes the operation of a computer program, the duration of its execution, from beginning to termination (compare compile time). Within KAS, runtime also refers to the virtual machine that manage the program written in a computer language while it is running is configured as adapter (server), up from 1. |
Table 10-3: Revision history for AKD PDMM EDS file for EtherNet/IP
|
Copyright © 2018 Kollmorgen |
|