Ethernet/IP IO Scanner (Client)

The KAS RuntimeIn computer science, runtime (or run-time) describes the operation of a computer program, the duration of its execution, from beginning to termination (compare compile time). Within KAS, runtime also refers to the virtual machine that manage the program written in a computer language while it is running includes a fully integrated EthernetEthernet is a large, diverse family of frame-based computer networking technologies that operate at many speeds for local area networks (LANs)/IP client driver for exchanging CIP"Common Industrial Protocol " The Common Industrial Protocol allows complete integration of control with information, multiple CIP Networks, and Internet technologies I/O assemblies as an Ethernet/IP scanner in your applications.

Data Exchange - Configuration

A dedicated configuration tool is integrated in the KAS IDE"Integrated development environment" An integrated development environment is a type of computer software that assists computer programmers in developing software. IDEs normally consist of a source code editor, a compiler and/or interpreter, build-automation tools, and a debugger.

  1. Double-click the FieldbusA Fieldbus is an industrial network system for real-time distributed control (e.g. CAN or Profibus). It is a way of connecting instruments in a plant design node in the project explorer to open it
  2. Click the Insert Configuration icon to add the Fieldbus configuration
  3. Then select the Ethernet/IP IO Scanner in the configuration selector

The configuration is represented as a tree:

  • Ethernet/IP IO Scanner
    • Server (an Ethernet/IP adapter device) (*)
      • IO Assembly (Originator to Target)
        • Exchanged Variable (*)
      • IO Assembly (Target to Originator)
        • Exchanged Variable (*)

(*) The items with this mark can appear several times in the configuration.

In addition to the IO configuration, explicit messaging can be performed using the blocks eipReadAttr and eipWriteAttr.

Configuration of the Server

Click the Insert Master icon to declare a server (slave adapter). Each server is identified by its IP address and an optional Description text.

Three blocks of data are exchanged with the server for each connection:

  • Outputs (originator to target)
  • Inputs (target to originator)
  • Configuration: a static block sent to the server at connection time.

The instance number for the configuration may be specified in the properties of the server.

Editing the Configuration Data Block

While most devices do not expect any configuration it may happen that some data is required. For this, double click on the server in the tree and press the Edit... button in the dialog box.

The configuration is entered as a list of items. Use the Type button to specify the number of items and their data types. Structured data types defined in the KAS IDE are supported. Simply enter values in the grid. In case you exchange multiple byte integers (e.g. WORD) you must specify whether the device expects little or big endian formatting.

Configuring an Assembly

Click the Insert Slave icon to declare a CIP I/O assembly. Each assembly is identified by:

Identifier Meaning
Type Direction of the I/O assembly. Can be one of:
  • Originator to Target (outputs)
  • Target to Originator (inputs)
Instance Instance of the CIP assembly
Config.instance The instance number of the configuration assembly. The default value is 100.
Size Data size in bytes
Connection type Type of the CIP connection. Can be Point To Point or MultiCast
Priority CIP priority: Low, High, Scheduled or Urgent
32 bit header Check this option if a 32 bit header is to be sent on notifications
RPI(ms) Minimum period for notification of changes, in milliseconds (range is 10 - 10000 ms)
Description Optional description text

Configuring Variables

IEC61131-3IEC 61131-3 is the third part of the open international standard IEC 61131. The current (second) edition was published in 2003. IEC 61131-3 currently defines five programming languages for programmable control systems It deals with programming languages and defines two graphical and two textual PLC programming language standards variables may be mapped on the data of the assembly. For each variable you must specify:

Identifier Meaning
Symbol The name of the IEC61131IEC standard for Programmable logic controllers (PLCs)-3 variable
Offset Offset in bytes in the assembly data
Bit Bit offset in the selected byte if format is "Bit"
Format Format of the data in the assembly
Mode Kind of data exchanged through the variable:
  • Data Exchange: a type of input or output data in the assembly
  • Server OK: indicates the status of the IP connection to the server
  • I/O connection OK: indicates the status of the CIP I/O connection
  • Last UCMM error: CIP code fo the last error occurred during a connection

  • The data limit is: 500 bytes of data maximum O(originator)->T(target) and 500 bytes of data maximum T(target) -> O(originator). This is based on the Ethernet/IP specification.

 


Stay Connected with Kollmorgen

Copyright © 2018 Kollmorgen