Tools Menu

Command

Description

Oscilloscope

Show the soft oscilloscope

Compile (Ctrl + B)

Compile the whole project

Compile & Download (Ctrl + F7) Compile the whole project and download it to the controller.
User Options

Open the User Options dialog box.

Table 5-5: Tools Menu Commands

User Options

AKD GUI Scope Settings

The check box found in this dialog enables/disables the “Load at startup” option in the AKD GUI"Graphical User Interface" A GUI is a type of user interface which allows people to interact with a computer and computer-controlled devices Scope “settings” tab.

AutoSave Recovery File Settings

This option Enables / Disables automatically saving project recovery files at a specified interval. Once set, this applies to all further project recovery files for the user. The stopwatch icon in the bottom right corner of the KAS IDE"Integrated development environment" An integrated development environment is a type of computer software that assists computer programmers in developing software. IDEs normally consist of a source code editor, a compiler and/or interpreter, build-automation tools, and a debugger indicates whether AutoSave Recovery Files is active or disabled . See About Auto Recovery for information about recovery files.

 


Stay Connected with Kollmorgen

Copyright © 2018 Kollmorgen