Window Menu

Command Shortcut Description

MDI/Tabbed Workspace

ALT+W

Toggle the workspace between the MDI"Multiple document interface" Graphical computer applications with an MDI are those whose windows reside under a single parent window (usually with the exception of modal windows), as opposed to all windows being separate from each other (single document interface). Advantages: - With MDI, a single menu bar and/or toolbar is shared between all child windows, reducing clutter and increasing efficient use of screen space - An application's child windows can be hidden/shown/minimized/maximized as a whole - Features such as "Tile" and "Cascade" can be implemented for the child windows and the tabbed mode

Cascade

ALT+C

Re-arrange all workspace children windows in cascade mode

Tile

ALT+T

Re-arrange all workspace children windows in tile mode

Reset IDE Layout Alt+R

This option will reset widgets to their default location and visibility. If an item is hidden or floating, it will be made visible and returned to its default position. The following interface items are affected by this option.

Table 5-6: Windows Menu Commands

 


Stay Connected with Kollmorgen

Copyright © 2018 Kollmorgen