ST Editor Keyboard Shortcuts
ST Editor (common)
| Shortcut | Command |
|---|---|
| Arrows | Move caretThe term caret is also sometimes used in graphical user interface terminology where it means a text insertion point indicator, frequently represented by a blinking vertical bar. In this context, it may be used interchangeably with the word cursor, although the latter term is often reserved for a mouse pointer |
| Shift + arrows | Selection |
| Ctrl + left/right arrow | Go to previous/next word |
| Shift + Ctrl + left/right arrow | Select previous/next word |
| Ctrl+F2 | Toggle Bookmark (Note that you first have to select the Network header) |
| Shift+F2 | Go to Next Bookmark |
| Ctrl+Shift+F2 | Go to Previous Bookmark |
| Ctrl + mouse-wheel or + / – on the keypad |
Zoom in / out |
Table 5-17: List of ST Shortcuts
ST Editor (when editing)
| Shortcut | Command |
|---|---|
| . | Select member of a structure or instance |
| Ctrl + Spacebar | Auto completion or Open the variable selector dialog |
| Ctrl + Shift + Spacebar | Opens a list of all the standard functions |
| Ctrl + J | Auto completion or Open the variable selector dialog (an alternative method) |
ST Editor (during debug)
| Shortcut | Command |
|---|---|
| * | Lock variable |
| / | Unlock variable |
| Shift + double-click | Force a variable |
| Spacebar | Toggle Boolean value or bring the dialog to force, lock, unlock the variable (equivalent of Shift + double click) |
|
Copyright © 2018 Kollmorgen |
|