ACTION#.SOURCE
Description
This keyword defines the input source for an action.
| Value | Description |
|---|---|
| 0 | No source |
| 1 | Mains ready |
| 2 | Digital Input |
| 3 | Digital Dio (Bidirectional) |
| 4 | Actual Velocity |
| 5 | Axis Faulted |
| 6 | Home Complete |
| 7 | Motion Task in Position |
| 8 | Controlled Stop Active |
| 9 | Software Limit |
| 10 | Move Complete |
| 11 | Position Error, Absolute |
| 12 | Axis Enabled |
| 13 | Analog Input |
| 14 | Current Command |
| 15 | Velocity Error |
| 16 | Velocity Command |
| 17 | Position Feedback |
| 18 | Axis Disable Immediately |
| 19 | Brake State |
| 20 | Ready to Operate (RTO/BTB) |
Versions
| Action | Version | Notes |
|---|---|---|
| Implemented | 02-00-00-000 |
General Information
|
Type |
Read/Write |
|
Units |
N/A |
|
Range |
0 to 17 |
|
Default Value |
0 (no source) |
|
Data Type |
Integer |
|
Stored in Non Volatile Memory |
Yes |
Variants Supported
All variants are supported
|
Copyright © 2018 Kollmorgen |
|