AXIS#.BODE.INJECTPOINT
Description
AXIS#.BODE.INJECTPOINT sets whether the excitation uses current or velocity excitation type.
|
AXIS#.BODE.INJECTPOINT |
Description |
|---|---|
|
0 |
None |
|
1 |
Current |
|
2 |
Velocity |
Example
Set AXIS1.BODE.INJECTPOINT to current:
-->AXIS1.BODE.INJECTPOINT 1
Get AXIS1.BODE.INJECTPOINT (already set to current):
-->AXIS1.BODE.INJECTPOINT 1
Versions
| Action | Version | Notes |
|---|---|---|
| Implemented | 02-00-00-000 |
General Information
|
Type |
Read/Write |
|
Units |
N/A |
|
Range |
0 to 2 |
|
Default Value |
0 |
|
Data Type |
Integer |
|
Stored in Non Volatile Memory |
Yes |
Variants Supported
All variants are supported
Fieldbus Information
| FieldbusA Fieldbus is an industrial network system for real-time distributed control (e.g. CAN or Profibus). It is a way of connecting instruments in a plant design | Parameter | Index | Sub-Index | Data Type | Float Scale | Units | Access | PDO Mappable |
|---|---|---|---|---|---|---|---|---|
| EtherCATEtherCAT is an open, high-performance Ethernet-based fieldbus system. The development goal of EtherCAT was to apply Ethernet to automation applications which require short data update times (also called cycle times) with low communication jitter (for synchronization purposes) and low hardware costs COE and CANopen | AXIS1.BODE.INJECTPOINT | 0x5001 | 0x1 | USINT | - | - | RW | False |
| AXIS2.BODE.INJECTPOINT | 0x5101 | 0x1 | USINT | - | - | RW | False |
|
Copyright © 2018 Kollmorgen |
|