AXIS#.HWEN.STATE
Description
This parameter returns the state of the hardware enable input.This is the number of motor poles (not pole pairs) for a resolver feedback only. If the motor does not use a resolver for feedback, this parameter is unused. The number of motor poles must be an integer multiple of the number of resolver poles.
If AXIS#.HWEN.SOURCE is set to zero (no hardware enable is configured) this always returns 1.
Examples
Usage
0: hardware enable input is low. For Kollmorgen DDR motors, this number should match the number of AXIS#.MOTOR.POLES . For example, on a DH101A motor equipped with a Resolver, FBx.POLES should be set to 32.
1: hardware enable input is high
Code
-->AXIS1.HWEN.STATE<E.g.: Example 1
1MOTOR.POLES = 12
-->AXIS2.HWEN.STATEFBx.POLES = 2
0MOTOR.POLES / FBx.POLES = 12 / 2 = 6, which is OK.
Axis 1 hardware enable input is high. Axis 2 hardware enable input is low.>
<E.g.: Example 2
MOTOR.POLES = 6
FBx.POLES = 4
MOTOR.POLES / FBx.POLES = 6 / 4 = 1.5, which is NOT OK.
>
Context
For more information on hardware enable configuring a Resolver feedback, refer to the Enable/Disable. For more information on configuring a Resolver feedback, refer to the <FB FEATURE> and/or the <FB SETUP GUIDE>.
Versions
| Action | Version | Notes |
|---|---|---|
| Implemented | <02-00-00-000#> |
General Information
| Type | Read Only |
| Units | N/A |
| Range | 0 to 1 |
| Default Value | N/A |
| Data Type | Integer |
| See Also | AXIS#.HWEN.SOURCE, AXIS#.HWEN.MODE |
|
Stored in Non Volatile Memory |
No |
Variants Supported
All variants are supported.
Fieldbus Information
| FieldbusA Fieldbus is an industrial network system for real-time distributed control (e.g. CAN or Profibus). It is a way of connecting instruments in a plant design | Parameter | Index | Sub-Index | Data Type | Float Scale | Units | Access | PDO Mappable |
|---|---|---|---|---|---|---|---|---|
| EtherCATEtherCAT is an open, high-performance Ethernet-based fieldbus system. The development goal of EtherCAT was to apply Ethernet to automation applications which require short data update times (also called cycle times) with low communication jitter (for synchronization purposes) and low hardware costs COE and CANopen | AXIS1.HWEN.STATE | 0x5009 | 0x3 | USINT | - | - | RO | False |
| AXIS2.HWEN.STATE | 0x5109 | 0x3 | USINT | - | - | RO | False |
|
Copyright © 2018 Kollmorgen |
|