AXIS#.HWLS.NEGSTATE
Description
Returns the state of the negative hardware limit switch
Examples
Usage
0: negative limit switch is low
1: negative limit switch is high
Code
Axis 1 negative limit switch is low. Axis 2 negative limit switch is high.
-->AXIS1.HWLS.NEGSTATE 0 -->AXIS2.HWLS.NEGSTATE 1
Context
For more information on limit switches, refer to Limits.
Versions
| Action | Version | Notes |
|---|---|---|
| Implemented | 02-00-00-000 |
General Information
| Type | Read Only |
| Units | N/A |
| Range | 0 to 1 |
| Default Value | N/A |
| Data Type | Integer |
| See Also | AXIS#.HWLS.NEGSOURCE |
| Stored in Non Volatile Memory | No |
Variants Supported
All variants are supported
Fieldbus Information
| FieldbusA Fieldbus is an industrial network system for real-time distributed control (e.g. CAN or Profibus). It is a way of connecting instruments in a plant design | Parameter | Index | Sub-Index | Data Type | Float Scale | Units | Access | PDO Mappable |
|---|---|---|---|---|---|---|---|---|
| EtherCATEtherCAT is an open, high-performance Ethernet-based fieldbus system. The development goal of EtherCAT was to apply Ethernet to automation applications which require short data update times (also called cycle times) with low communication jitter (for synchronization purposes) and low hardware costs COE and CANopen | AXIS1.HWLS.NEGSTATE | 0x5015 | 0x1 | USINT | - | - | RO | True |
| AXIS2.HWLS.NEGSTATE | 0x5115 | 0x1 | USINT | - | - | RO | True |
|
Copyright © 2018 Kollmorgen |
|