AXIS#.HWLS.POSSTATE

Description

Returns the state of the positive hardware limit switch

Examples

Usage

0: positive limit switch is low

1: positive limit switch is high

Code

Axis 1 positive limit switch is low. Axis 2 positive limit switch is high.

-->AXIS1.HWLS.POSSTATE
0
-->AXIS2.HWLS.POSSTATE
1

Context

For more information on limit switches, refer to Limits.

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type Read Only
Units N/A
Range 0 to 1
Default Value N/A
Data Type Integer
See Also AXIS#.HWLS.POSSOURCE
Stored in Non Volatile Memory No

Variants Supported

All variants are supported

Fieldbus Information

FieldbusA Fieldbus is an industrial network system for real-time distributed control (e.g. CAN or Profibus). It is a way of connecting instruments in a plant design Parameter Index Sub-Index Data Type Float Scale Units Access PDO Mappable
EtherCATEtherCAT is an open, high-performance Ethernet-based fieldbus system. The development goal of EtherCAT was to apply Ethernet to automation applications which require short data update times (also called cycle times) with low communication jitter (for synchronization purposes) and low hardware costs COE and CANopen AXIS1.HWLS.POSSTATE 0x5015 0x2 USINT - - RO True
AXIS2.HWLS.POSSTATE 0x5115 0x2 USINT - - RO True

 


Stay Connected with Kollmorgen

Copyright © 2018 Kollmorgen