AXIS#.IL.FBSOURCE
Description
This parameter selects the feedback source that current loop uses for commutation angle calculation.
Feedback Sources/Connectors:
1 selects FB1 (connector X1)
2 selects FB2 (connector X2)
3 selects FB3 (connector X23)
4 selects FB4 (connector X21)
5 selects FB5 (connector X22)
Versions
| Action | Version | Notes |
|---|---|---|
| Implemented | 02-00-00-000 |
General Information
|
Type |
Read/Write |
|
Units |
N/A |
|
Range |
1 to 5 |
|
Default Value |
1 |
|
Data Type |
Integer |
|
Stored in Non Volatile Memory |
Yes |
Variants Supported
All variants are supported
Fieldbus Information
| FieldbusA Fieldbus is an industrial network system for real-time distributed control (e.g. CAN or Profibus). It is a way of connecting instruments in a plant design | Parameter | Index | Sub-Index | Data Type | Float Scale | Units | Access | PDO Mappable |
|---|---|---|---|---|---|---|---|---|
| EtherCATEtherCAT is an open, high-performance Ethernet-based fieldbus system. The development goal of EtherCAT was to apply Ethernet to automation applications which require short data update times (also called cycle times) with low communication jitter (for synchronization purposes) and low hardware costs COE and CANopen | AXIS1.IL"Instruction list" This is a low-level language and resembles assembly.FBSOURCE | 0x500A | 0x6 | USINT | - | - | RW | False |
| AXIS2.IL.FBSOURCE | 0x510A | 0x6 | USINT | - | - | RW | False |
|
Copyright © 2018 Kollmorgen |
|