AXIS#.IL.IFOLD

Description

Two current foldback algorithms run in parallel in the drive: the drive foldback algorithm and the motor foldback algorithm. Each algorithm uses different sets of parameters.

Each algorithm has its own foldback current limit, AXIS#.IL"Instruction list" This is a low-level language and resembles assembly.DIFOLD and AXIS#.IL.MIFOLD. The overall foldback current limit is the minimum of the two at any given moment.

AXIS#.IL.IFOLD = min (AXIS#.IL.DIFOLD, AXIS#.IL.MIFOLD).

AXIS#.IL.DIFOLD is an artificial current, which can be higher or lower than the drive or motor peak current. When AXIS#.IL.IFOLD becomes lower than the existing current limit (such as AXIS#.IL.LIMITP ), it becomes the active current limit.

Versions

Action Version Notes
Implemented 02-00-00-000
     

General Information

Type

Read Only

Units

A

Range

0 to 2,147,483.647 A

Default Value

N/A

Data Type

Float

See Also

Foldback

Stored in Non Volatile Memory

No

Variants Supported

All variants are supported

Fieldbus Information

FieldbusA Fieldbus is an industrial network system for real-time distributed control (e.g. CAN or Profibus). It is a way of connecting instruments in a plant design Parameter Index Sub-Index Data Type Float Scale Units Access PDO Mappable
EtherCATEtherCAT is an open, high-performance Ethernet-based fieldbus system. The development goal of EtherCAT was to apply Ethernet to automation applications which require short data update times (also called cycle times) with low communication jitter (for synchronization purposes) and low hardware costs COE and CANopen AXIS1.IL.IFOLD 0x500A 0xC DINT 1000:1 - RO False
AXIS2.IL.IFOLD 0x510A 0xC DINT 1000:1 - RO False

 


Stay Connected with Kollmorgen

Copyright © 2018 Kollmorgen