AXIS#.MOTOR.BRAKE
Description
The AXIS#.MOTOR.BRAKE parameter notifies the firmware whether a brake exists or not. It does not apply or release the brake. If a brake is found to be present, the firmware considers hardware indications regarding the brake circuits (such as open circuit or short circuit). If a brake does not exist, then the firmware ignores the hardware indications since they are irrelevant.
|
Value |
Status |
|---|---|
|
0 |
Motor brake does not exist. |
|
1 |
Motor brake exists and brake hardware circuitry checks are enabled. |
| 100 | For special, low current, brake applications, brake faults are bypassed with this setting. |
When the axis is enabled, setting AXIS#.MOTOR.BRAKE to 1 when no motor brake exists creates a fault.
-
-
This parameter is automatically configured for (Undefined variable: MyVariables.CompanyName) motors when MOTOR.AUTOSET=1 and motor memory version is 0.2 or greater.
Examples
Context
For more information see Brake and Motor.
Versions
| Action | Version | Notes |
|---|---|---|
| Implemented | 02-00-00-000 |
General Information
|
Type |
Read/Write |
|
Units |
N/A |
|
Range |
0, 1, 100 |
|
Default Value |
0 |
|
Data Type |
Integer |
|
See Also |
N/A |
|
Stored in Non Volatile Memory |
Yes |
Variants Supported
All variants are supported
Fieldbus Information
| FieldbusA Fieldbus is an industrial network system for real-time distributed control (e.g. CAN or Profibus). It is a way of connecting instruments in a plant design | Parameter | Index | Sub-Index | Data Type | Float Scale | Units | Access | PDO Mappable |
|---|---|---|---|---|---|---|---|---|
| EtherCATEtherCAT is an open, high-performance Ethernet-based fieldbus system. The development goal of EtherCAT was to apply Ethernet to automation applications which require short data update times (also called cycle times) with low communication jitter (for synchronization purposes) and low hardware costs COE and CANopen | AXIS1.MOTOR.BRAKE | 0x500B | 0x8 | USINT | - | - | RW | False |
| AXIS2.MOTOR.BRAKE | 0x510B | 0x8 | USINT | - | - | RW | False |
|
Copyright © 2018 Kollmorgen |
|