AXIS#.MOTOR.PHASE
Description
This parameter is the relative alignment of the feedback to the motor coils. For (Undefined variable: MyVariables.CompanyName) motors, the feedback and coils are aligned, and AXIS#.MOTOR.PHASE may be set to 0.
-
-
If MOTOR.AUTOSET = 1 and motor memory version is 0.2 or greater, this parameter is automatically configured for Kollmorgen motors.
Context
For more information see Motor.
Versions
| Action | Version | Notes |
|---|---|---|
| Implemented | 02-00-00-000 |
General Information
|
Type |
Read/Write |
|
Units |
Electrical degrees |
|
Range |
0 to 360 |
|
Default Value |
0 |
|
Data Type |
Integer |
|
See Also |
N/A |
|
Stored in Non Volatile Memory |
Yes |
Variants Supported
All variants are supported
Fieldbus Information
| FieldbusA Fieldbus is an industrial network system for real-time distributed control (e.g. CAN or Profibus). It is a way of connecting instruments in a plant design | Parameter | Index | Sub-Index | Data Type | Float Scale | Units | Access | PDO Mappable |
|---|---|---|---|---|---|---|---|---|
| EtherCATEtherCAT is an open, high-performance Ethernet-based fieldbus system. The development goal of EtherCAT was to apply Ethernet to automation applications which require short data update times (also called cycle times) with low communication jitter (for synchronization purposes) and low hardware costs COE and CANopen | AXIS1.MOTOR.PHASE | 0x500B | 0x15 | UINT | - | - | RW | False |
| AXIS2.MOTOR.PHASE | 0x510B | 0x15 | UINT | - | - | RW | False |
|
Copyright © 2018 Kollmorgen |
|