AXIS#.SM.DEC
Description
Sets the deceleration ramp for service motion if set to greater than 0.
-
- AXIS#.SM.DEC is limited by AXIS#.DEC
Versions
| Action | Version | Notes |
|---|---|---|
| Implemented | 02-00-00-000 | |
General Information
|
Type |
Read/Write |
|
Units |
Rotary: RPM"Revolutions per minute" Is a unit of frequency of rotation: the number of full rotations completed in one minute around a fixed axis. It is used as a measure of rotational speed of a mechanical component/s, RPS/s, deg/s2, (custom units)/s2, rad/s2 Linear: counts/s2, mm/s2, µm/s2 , (custom units)/s2 See Acceleration Units for details. |
|
Range |
Depends on units. See Acceleration Units for details. |
|
Default Value |
30,000 rpm/s Depends on units. See Acceleration Units for details. |
|
Data Type |
Float |
| See Also | |
|
Stored in Non Volatile Memory |
Yes |
Variants Supported
All variants are supported
|
Copyright © 2018 Kollmorgen |
|