AXIS#.VL.CMD

Description

AXIS#.VL.CMD returns the actual velocity command as it is received in the velocity loop entry after all velocity limits (such as AXIS#.VL.LIMITN and AXIS#.VL.LIMITP ). See velocity loop design diagram for more details.


  • When in Position Mode, VL.CMD contains the output of both desired trajectory velocity as well as the output of the position loop, if the pure trajectory velocity is deisred, refer to AXIS#.MT.VCMD.

    In Velocity Mode, VL.CMD will be equal to only the trajectory velocity command.

Versions

Action Version Notes
Implemented 02-00-00-000
     

General Information

Type

Read Only

Units

Depends on AXIS#.UNIT.VROTARY (pg 1) or AXIS#.UNIT.VLINEAR (pg 1)

Rotary: rpm, rps, deg/s, (custom units)/s, rad/s

Linear: counts/s, mm/s, µm/s, (custom units)/s

Range

N/A

Default Value

N/A

Data Type

Float

Stored in Non Volatile Memory

No

Variants Supported

All variants are supported

Related Topics

Velocity Loop

Position Loop

 


Stay Connected with Kollmorgen

Copyright © 2018 Kollmorgen