AXIS#.VL.THRESH

Description

AXIS#.VL.THRESH sets the user overspeed fault threshold. This threshold becomes the overall overspeed fault threshold (AXIS#.VL.VFTHRESH) if it is less than the motor speed threshold (1.2 x AXIS#.MOTOR.VMAX), and for AXIS#.MOTOR.TYPE = 6 if it is less than the motor back EMF overspeed threshold ((1.02 x 1000 x VBUS.OVFTHRESH) / (AXIS#.MOTOR.KE x sqrt(2))).

The value is considered an absolute value, hence it applies for both negative and positive velocities.

Example

AXIS#.VL.THRESH is set to 600 rpm. A velocity (AXIS#.VL.FB ) of 700 rpm will generate an over speed fault.

Versions

Action Version Notes
Implemented 02-00-00-000
     

General Information

Type

Read/Write

Units

Rotary: RPM"Revolutions per minute" Is a unit of frequency of rotation: the number of full rotations completed in one minute around a fixed axis. It is used as a measure of rotational speed of a mechanical component, RPS, deg/s, (custom units)/s, rad/s

Linear: counts/s, mm/s, µm/s, (custom units)/s
See Velocity Units for details.

Range

Depends on units. See Velocity Range for details.

Default Value

3,600 RPM

Depends on units. See Velocity Units for details.

Data Type

Float

Stored in Non Volatile Memory

Yes

Variants Supported

All variants are supported

Fieldbus Information

FieldbusA Fieldbus is an industrial network system for real-time distributed control (e.g. CAN or Profibus). It is a way of connecting instruments in a plant design Parameter Index Sub-Index Data Type Float Scale Units Access PDO Mappable
EtherCATEtherCAT is an open, high-performance Ethernet-based fieldbus system. The development goal of EtherCAT was to apply Ethernet to automation applications which require short data update times (also called cycle times) with low communication jitter (for synchronization purposes) and low hardware costs COE and CANopen AXIS1.VL.THRESH 0x5011 0x8 UDINT - Velocity RW False
AXIS2.VL.THRESH 0x5111 0x8 UDINT - Velocity RW False

 


Stay Connected with Kollmorgen

Copyright © 2018 Kollmorgen