DOUT#.STATEU
Description
Gets or sets the user command state of the specified digital output when DOUT#.SOURCE = 0 (user).
| Value | Description |
|---|---|
| 0 - Deactivated | DOUT#.STATE = 0, voltage removed on IO pin |
| 1 - Activated | DOUT#.STATE = 1, voltage applied on IO pin |
Examples
Usage
When DOUT#.SOURCE = 0 (user) then the corresponding DOUT#.STATEU can be set to drive the output at the IO pin.
Code
--> DOUT1.SOURCE 0 //user --> DOUT1.STATEU 0 --> DOUT1.STATE 0 --> DOUT1.STATEU 1 --> DOUT1.STATE 1
Context
For more information see Digital I/O.
Versions
| Action | Version | Notes |
|---|---|---|
| Implemented | 02-00-00-000 |
General Information
| Type | Read/Write |
| Units | N/A |
| Range | 0 to 1 |
| Default Value | N/A |
| Data Type | Integer |
| See Also | |
|
Stored in Non Volatile Memory |
No |
Variants Supported
All variants are supported
Fieldbus Information
|
Copyright © 2018 Kollmorgen |
|