AXIS#.DBILIMIT
Description
This parameter sets the maximum amplitude of the current for dynamic braking.
Example
Setting AXIS#.DBILIMIT to 2 limits the dynamic brake current to 2 Arms.
Versions
| Action | Version | Notes |
|---|---|---|
| Implemented | 02-00-00-000 |
General Information
|
Type |
Read/Write |
|
Units |
Arms |
|
Range |
0 to minimum of drive peak current (IPEAK) and motor peak current (AXIS#.MOTOR.IPEAK). |
|
Default Value |
Minimum of drive continuous current (ICONT) and motor continuous current (AXIS#.MOTOR.ICONT). |
|
Data Type |
Float |
|
Stored in Non Volatile Memory |
Yes |
Variants Supported
All variants are supported
Fieldbus Information
| FieldbusA Fieldbus is an industrial network system for real-time distributed control (e.g. CAN or Profibus). It is a way of connecting instruments in a plant design | Parameter | Index | Sub-Index | Data Type | Float Scale | Units | Access | PDO Mappable |
|---|---|---|---|---|---|---|---|---|
| EtherCATEtherCAT is an open, high-performance Ethernet-based fieldbus system. The development goal of EtherCAT was to apply Ethernet to automation applications which require short data update times (also called cycle times) with low communication jitter (for synchronization purposes) and low hardware costs COE and CANopen | AXIS1.DBILIMIT | 0x5000 | 0x7 | UDINT | 1000:1 | - | RW | False |
| AXIS2.DBILIMIT | 0x5100 | 0x7 | UDINT | 1000:1 | - | RW | False |
|
Copyright © 2018 Kollmorgen |
|