AXIS#.OPMODE
Description
AXIS#.OPMODE specifies the operation mode of the drive. You must also use AXIS#.CMDSOURCE to set the source of the command to the drive.
The operation mode values can be set as follows:
|
Mode |
Description |
|---|---|
|
0 |
Current (torqueTorque is the tendency of a force to rotate an object about an axis. Just as a force is a push or a pull, a torque can be thought of as a twist) operation mode |
|
1 |
Velocity operation mode |
|
2 |
Position operation mode |
AXIS#.OPMODE can be changed while the drive is enabled or disabled. If you are using the terminal to change the operation mode, then it is recommended that you disable the drive before changing the operation mode. If you change the operation mode from the terminal while the drive is enabled, the system may experience a step change in demand.
Example
Set the source of the command to a TCP/IP channel and the desired operation mode to velocity:
-->CMDSOURCE 0
-->OPMODE 1
Versions
| Action | Version | Notes |
|---|---|---|
| Implemented | 02-00-00-000 |
General Information
|
Type |
Read/Write |
|
Units |
N/A |
|
Range |
0 to 2 |
|
Default Value |
0 |
|
Data Type |
Integer |
|
Stored in Non Volatile Memory |
Yes |
Variants Supported
All variants are supported
Fieldbus Information
| FieldbusA Fieldbus is an industrial network system for real-time distributed control (e.g. CAN or Profibus). It is a way of connecting instruments in a plant design | Parameter | Index | Sub-Index | Data Type | Float Scale | Units | Access | PDO Mappable |
|---|---|---|---|---|---|---|---|---|
| EtherCATEtherCAT is an open, high-performance Ethernet-based fieldbus system. The development goal of EtherCAT was to apply Ethernet to automation applications which require short data update times (also called cycle times) with low communication jitter (for synchronization purposes) and low hardware costs COE and CANopen | AXIS1.OPMODE | 0x5000 | 0x5 | USINT | - | - | RW | False |
| AXIS2.OPMODE | 0x5100 | 0x5 | USINT | - | - | RW | False |
|
Copyright © 2018 Kollmorgen |
|