AIN.ISCALE
Description
AIN.ISCALE sets the analog current scale factor that scales the analog input (AIN.VALUE) for DRV.OPMODE = 1 (analog torqueTorque is the tendency of a force to rotate an object about an axis. Just as a force is a push or a pull, a torque can be thought of as a twist mode).
The actual analog input will be limited by the application current limit (IL.LIMITN and IL.LIMITP ).
General Information
|
Type |
NV Parameter |
|
Units |
A/V |
|
Range |
0.001 to 22.4 A/V |
|
Default Value |
0.001 A/V |
|
Data Type |
Float |
|
Start Version |
M_01-01-01-000 |
Variants Supported
|
Index/Subindex |
Object Start Version |
|
|---|---|---|
|
5002h/0 |
M_01-01-01-000 |
Related Topics
|
Copyright © 2018 Kollmorgen |
|