AOUT.CUTOFF

Description

AOUT.CUTOFF sets the cutoff frequency in Hz for a single-pole low-pass
filter on the Analog Output.

A value of 0 Hz will turn off the filter and will allow all frequencies to pass through.

The filter can be used with all modes of Analog Output.

General Information

Type

NV Parameter

Units

Hz

Range

0 to 10,000 Hz

Default Value

0 Hz

Data Type

Float

Start Version

M_01-04-01

FieldbusA Fieldbus is an industrial network system for real-time distributed control (e.g. CAN or Profibus). It is a way of connecting instruments in a plant design

Index/Subindex

Object Start Version

EtherCATEtherCAT is an open, high-performance Ethernet-based fieldbus system. The development goal of EtherCAT was to apply Ethernet to automation applications which require short data update times (also called cycle times) with low communication jitter (for synchronization purposes) and low hardware costs COE and CANopen

3470h/6

M_01-04-01-000

Related Topics

Analog Output

 


Stay Connected with Kollmorgen

Copyright © 2018 Kollmorgen