CMPx.ARM

Description

Use this keyword to arm or disarm a Compare setpointSetpoint is the target value that an automatic control system, for example PID controller, will aim to reach. The setpoint value will only be compared against the Compare source (CMPx.SOURCE) if that setpoint is armed. If they match, an output pulse will be generated.

An error will be generated if CMPx.SOURCE, CMPx.MODBOUND1, CMPx.MODBOUND2, CMPx.WIDTH, and CMPx.MODEN are not set prior to enabling CMPx.ARM. If CMPx.SETPOINT is not set prior to enabling CMPx.ARM, the compare will trigger at the last set value, or the default value of 0 if the drive has been power cycled.

Example

The following example arms setpoint 3 for CMP1.

-->CMP1.ARM 3 1

General Information

Type

NV Parameter

Units

N/A

Range

Argument 1: 0 to 7

Argument 2: 0 (Disarm) or 1 (Arm)

Default Value

0 (Disarm)

Data Type

Argument 1: Integer

Argument 2: Integer

Start Version

M_01-13-00-000

Compare functionality is supported on hardware revisions D, DB, DA, and higher depending on the drive type. Check the label on the side of the drive to ensure the AKD meets one of the following requirements.

AKD Type Hardware Revision Supported
AKD Revision D or higher
AKD PDMM Revision DB or higher
AKD-T-IC"Integrated Circuits" Miniaturized electronic circuits (consisting mainly of semiconductor devices, as well as passive components) that have been manufactured in the surface of a thin substrate of semiconductor material Revision DA or higher
FieldbusA Fieldbus is an industrial network system for real-time distributed control (e.g. CAN or Profibus). It is a way of connecting instruments in a plant design Index/Subindex Object Start Version

EtherCATEtherCAT is an open, high-performance Ethernet-based fieldbus system. The development goal of EtherCAT was to apply Ethernet to automation applications which require short data update times (also called cycle times) with low communication jitter (for synchronization purposes) and low hardware costs COE and CANopen

34C0h/1

CMP0.ARM

M_01-13-00-000
34C1h/1

CMP1.ARM

Related Topics

Compare Engines

CMPx.SETPOINT | CMPx.SOURCE

 


Stay Connected with Kollmorgen

Copyright © 2018 Kollmorgen