CMPx.MODE
Description
This keyword sets the mode for a Compare setpointSetpoint is the target value that an automatic control system, for example PID controller, will aim to reach to either single-shot or continuous. Single-shot automatically disarms the setpoint after a pulse is generated. Continuous mode will keep the setpoint armed after a pulse has been generated.
Example
The following example sets the mode for setpoint 3 to single-shot.
-->CMP1.MODE 7 0
General Information
|
Type |
NV Parameter |
|
Units |
None |
|
Range |
Argument 1: 0 to 7 Argument 2: 0 (Single-shot) or 1 (Continuous) |
|
Default Value |
1 (Continuous) |
|
Data Type |
Argument 1: Integer Argument 2: Integer |
|
Start Version |
M_01-13-00-000 |
Compare functionality is supported on hardware revisions D, DB, DA, and higher depending on the drive type. Check the label on the side of the drive to ensure the AKD meets one of the following requirements.
| AKD Type | Hardware Revision Supported |
|---|---|
| AKD | Revision D or higher |
| AKD PDMM | Revision DB or higher |
| AKD-T-IC"Integrated Circuits" Miniaturized electronic circuits (consisting mainly of semiconductor devices, as well as passive components) that have been manufactured in the surface of a thin substrate of semiconductor material | Revision DA or higher |
| FieldbusA Fieldbus is an industrial network system for real-time distributed control (e.g. CAN or Profibus). It is a way of connecting instruments in a plant design | Index/Subindex | Object Start Version | |
|---|---|---|---|
| 34ADh/1 | CMP0.MODE 0 | M_01-13-00-000 | |
| 34AAh/2 | CMP0.MODE 1 | ||
| 34AAh/3 | CMP0.MODE 2 | ||
| 34AAh/4 | CMP0.MODE 3 | ||
| 34AAh/5 | CMP0.MODE 4 | ||
| 34AAh/6 | CMP0.MODE 5 | ||
| 34AAh/7 | CMP0.MODE 6 | ||
| 34AAh/8 | CMP0.MODE 7 | ||
|
34BDh/1 |
CMP1.MODE 0 | ||
|
34BAh/2 |
CMP1.MODE 1 | ||
|
34BAh/3 |
CMP1.MODE 2 | ||
|
34BAh/4 |
CMP1.MODE 3 | ||
|
34BAh/5 |
CMP1.MODE 4 | ||
|
34BAh/6 |
CMP1.MODE 5 | ||
|
34BAh/7 |
CMP1.MODE 6 | ||
|
34BAh/8 |
CMP1.MODE 7 | ||
Related Topics
|
Copyright © 2018 Kollmorgen |
|