COGCOMP.SAVE
Description
This parameter saves the current cogging compensation table (COGCOMP.CORRECTIONTABLE) from RAM to NV memory. On next drive boot, the cogging compensation table will be initialized with the stored entries from NV.
General Information
This content is not applicable to KAS, using either a PAC"Programmable Automation Controller" PAC is a compact controller that combines the features and capabilities of a PC-based control system with that of a typical programmable logic controller (PLC). A PAC thus provides not only the reliability of a PLC, but also the task flexibility and computing power of a PC. Additionally, because they function and communicate over popular network interface protocols, PACs are able to transfer data from the machines they control to other machines and components in a networked control system or a PDMM.
|
Type |
Command |
|
Units |
N/A |
|
Range |
N/A |
|
Default Value |
N/A |
|
Data Type |
N/A |
|
Start Version |
M_01-14-07-000 |
Related Topics
|
Copyright © 2018 Kollmorgen |
|