DIN1.MODE TO DIN7.MODE
Description
This parameter sets the functionality of the digital inputs. Digital inputs and corresponding X7 and X8 pin connectors are described in the AKD Installation Manual, section 8.16.4, Digital Inputs. The table below summarizes the digital input modes; for detailed descriptions of each mode, see Digital Inputs and Outputs.
|
DINx.MODE |
Description |
Task |
|---|---|---|
|
No function; off |
None |
|
|
Fault reset |
Background |
|
|
Start motion task (use DINx.PARAM for this task) |
1 KHz |
|
|
Start jog |
Background |
|
|
7 |
Reserved |
None |
|
Zero latch |
Background |
|
|
Command buffer |
Background |
|
|
Control fault relay |
Background |
|
|
Home reference |
1 kHz |
|
|
12 |
Reserved |
None |
|
1 kHz |
||
|
14 |
Reserved |
None |
|
Quick stop |
Background |
|
|
Activate electronic gear position shift |
Background |
|
|
Positive limit switch |
4 kHz |
|
|
Negative limit switch |
4kHz |
|
|
Brake release |
Background |
|
|
Current limit |
4 kHz |
|
|
Opmode and Command Source switch |
Background |
|
|
Change algebraic sign of the measured analog input voltage. |
1 kHz |
|
| 24 | Reserved | 1 kHz |
| 25 | Controlled stop without re-enable. | 1 kHz |
| 26 | Suspend Motion | 1 kHz |
General Information
|
Type |
R/W Parameter |
|
Units |
N/A |
|
Range |
0 to 26 |
|
Default Value |
0 |
|
Data Type |
Integer |
|
Start Version |
M_01-00-00-000 |
| FieldbusA Fieldbus is an industrial network system for real-time distributed control (e.g. CAN or Profibus). It is a way of connecting instruments in a plant design | Index/Subindex | Object Start Version | |
|---|---|---|---|
|
3562h/0 |
M_01-00-00-000 | ||
|
3565h/0 |
|||
|
3568h/0 |
|||
|
356Bh/0 |
|||
|
36F6h/0 |
|||
|
36F9h/0 |
|||
|
36FCh/0 |
|||
|
DIN1.MODE TO DIN6.MODE |
|||
Related Topics
Command Buffer
|
Copyright © 2018 Kollmorgen |
|