DRV.FAULTDISPLAYMODE
Description
DRV.FAULTDISPLAYMODE sets the LED display behavior when faults are present.
| Value | Description |
|---|---|
| 0 | Only the highest priority fault is displayed. |
| 1 | All faults displayed. |
General Information
|
Type |
NV Parameter |
|
Units |
N/A |
|
Range |
0 to 1 |
|
Default Value |
0 |
|
Data Type |
Integer |
|
Start Version |
M_01-13-00-000 |
| FieldbusA Fieldbus is an industrial network system for real-time distributed control (e.g. CAN or Profibus). It is a way of connecting instruments in a plant design | Index/Subindex | Object Start Version |
|---|---|---|
|
53C7h |
M_01-13-00-000 |
Related Topics
|
Copyright © 2018 Kollmorgen |
|