DRV.FAULT1 to DRV.FAULT10
Description
These parameters are holding registers where any active faults will be kept. A value of zero represents that no fault is present. Non-zero values correspond to specific fault codes in the drive (see fault and warning messages). The registers are populated in the order of when the fault occurs (DRV.FAULT1, DRV.FAULT2, DRV.FAULT3, and so on).
Notes:
- DRV.FAULT1 to DRV.FAULT10 are only updated when DRV.FAULT1 is read. If the fault does not exist when DRV.FAULT1 is read, it may not be registered in DRV.FAULT2 to DRV.FAULT10.
- If DRV.FAULT1 value is 0, then the drive does not have any faults.
- Only active faults are shown. This is not a fault history.
- These registers are an alternative to the string type parameter DRV.FAULTS, so that fieldbusses and AKD BASIC users have easier access to the details of the faults in the drive.
- Warnings are not shown in the registers, only faults.
General Information
|
Type |
R/O |
|
Units |
N/A |
|
Range |
Any supported fault code or 0. |
|
Default Value |
N/A |
|
Data Type |
Integer |
|
Start Version |
M_01-06-00-000 |
| FieldbusA Fieldbus is an industrial network system for real-time distributed control (e.g. CAN or Profibus). It is a way of connecting instruments in a plant design | Index/Subindex | Object Start Version | |
|---|---|---|---|
|
2001h/1 |
DRV.FAULT1 |
M_01-00-00-000 | |
|
2001h/2 |
DRV.FAULT2 | ||
|
2001h/3 |
DRV.FAULT3 | ||
|
2001h/4 |
DRV.FAULT4 | ||
|
2001h/5 |
DRV.FAULT5 | ||
|
2001h/6 |
DRV.FAULT6 | ||
|
2001h/7 |
DRV.FAULT7 | ||
|
2001h/8 |
DRV.FAULT8 | ||
|
2001h/9 |
DRV.FAULT9 | ||
|
2001h/A |
DRV.FAULT10 | ||
Related Topics
|
Copyright © 2018 Kollmorgen |
|